Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ArrayValue Class / NumValues Property


In This Topic
    NumValues Property
    In This Topic
    NumValues in the Array.
    Syntax
    Public Property NumValues As System.Integer
    public System.int NumValues {get; set;}
    public:
    property System.int NumValues {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also