Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmInfo Class / Severity Property


In This Topic
    Severity Property (AlarmInfo)
    In This Topic
    Syntax
    Public Property Severity As System.UInteger
    public System.uint Severity {get; set;}
    public:
    property System.uint Severity {
       System.uint get();
       void set (    System.uint value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also