Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmFields Class / EventCategory Property


In This Topic
    EventCategory Property (AlarmFields)
    In This Topic
    Syntax
    Public Property EventCategory As AlarmField
    public AlarmField EventCategory {get; set;}
    public:
    property AlarmField^ EventCategory {
       AlarmField^ get();
       void set (    AlarmField^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also