Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmFields Class / AllFields Property


In This Topic
    AllFields Property
    In This Topic
    Syntax
    Public Property AllFields As System.Boolean
    public System.bool AllFields {get; set;}
    public:
    property System.bool AllFields {
       System.bool get();
       void set (    System.bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also