Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / Opening Event


In This Topic
    Opening Event
    In This Topic
    Occurs when a connection is being established with a Historian server.
    Syntax
    Public Event Opening As System.EventHandler
    public event System.EventHandler Opening
    public:
    event System.EventHandler^ Opening
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also