Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnPublishSetDestinationServer Method
Indication of how the request was processed.


In This Topic
    OnPublishSetDestinationServer Method
    In This Topic
    Invoked by the remote server to transmit the result of setting a destination server name.
    Syntax
    Public Sub OnPublishSetDestinationServer( _
       ByVal status As Status _
    ) 
    public void OnPublishSetDestinationServer( 
       Status status
    )
    public:
    void OnPublishSetDestinationServer( 
       Status status
    ) 

    Parameters

    status
    Indication of how the request was processed.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also