Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnArchiveChanged Method
The type of archive change.
The list of impacted archives.


In This Topic
    OnArchiveChanged Method
    In This Topic
    Invoked by the remote server to transmit archive subscription details.
    Syntax
    Public Sub OnArchiveChanged( _
       ByVal changetype As ChangeType, _
       ByVal archives As System.Collections.Generic.List(Of Archive) _
    ) 
    public void OnArchiveChanged( 
       ChangeType changetype,
       System.Collections.Generic.List<Archive> archives
    )
    public:
    void OnArchiveChanged( 
       ChangeType changetype,
       System.Collections.Generic.List<Archive^>^ archives
    ) 

    Parameters

    changetype
    The type of archive change.
    archives
    The list of impacted archives.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also