Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiFieldValue Class / NumFields Property


In This Topic
    NumFields Property
    In This Topic
    NumFields in the MultiFiled Type.
    Syntax
    Public Property NumFields As System.Integer
    public System.int NumFields {get; set;}
    public:
    property System.int NumFields {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also