Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MessageCriteria Class / Start Property


In This Topic
    Start Property
    In This Topic
    Establish a message start time for a query.
    Syntax
    Public Property Start As System.Date
    public System.DateTime Start {get; set;}
    public:
    property System.DateTime Start {
       System.DateTime get();
       void set (    System.DateTime value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also