Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / MaxUsers Field


In This Topic
    MaxUsers Field
    In This Topic
    The maximum number of licensed user connections.
    Syntax
    Public MaxUsers As System.UInteger
    public System.uint MaxUsers
    public:
    System.uint MaxUsers
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also