Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / ActualUsers Field


In This Topic
    ActualUsers Field
    In This Topic
    The current number of active user connections.
    Syntax
    Public ActualUsers As System.UInteger
    public System.uint ActualUsers
    public:
    System.uint ActualUsers
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also