Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSet Class / AdministratorSecurityGroup Property


In This Topic
    AdministratorSecurityGroup Property (EnumeratedSet)
    In This Topic
    AdministratorSecurityGroup
    Syntax
    Public Property AdministratorSecurityGroup As System.String
    public System.string AdministratorSecurityGroup {get; set;}
    public:
    property System.String^ AdministratorSecurityGroup {
       System.String^ get();
       void set (    System.String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also