Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ElementValue Class / Value Property


In This Topic
    Value Property (ElementValue)
    In This Topic
    Value of the ElementValue.
    Syntax
    Public Property Value As System.Object
    public System.object Value {get; set;}
    public:
    property System.Object^ Value {
       System.Object^ get();
       void set (    System.Object^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also