Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / UserStatus Property


In This Topic
    UserStatus Property
    In This Topic
    Optional, user-defined status bits.
    Syntax
    Public Property UserStatus As System.UShort
    public System.ushort UserStatus {get; set;}
    public:
    property System.ushort UserStatus {
       System.ushort get();
       void set (    System.ushort value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also