Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / StatusMask Field


In This Topic
    StatusMask Field
    In This Topic
    Bit-mask for extracting quality status.
    Syntax
    Public Const StatusMask As System.UInteger
    public const System.uint StatusMask
    public:
    const System.uint StatusMask
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also