Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / CCriteriaStringModifier Class / CriteriaFromString Method


In This Topic
    CriteriaFromString Method (CCriteriaStringModifier)
    In This Topic
    Retrieves the sampling mode, calculation mode and query modifiers from criteriaString
    Syntax
    Public Function CriteriaFromString( _
       ByVal criteriaString As System.String, _
       ByRef criteria As DataCriteria _
    ) As System.Boolean
    public System.bool CriteriaFromString( 
       System.string criteriaString,
       ref DataCriteria criteria
    )
    public:
    System.bool CriteriaFromString( 
       System.String^ criteriaString,
       DataCriteria^% criteria
    ) 

    Parameters

    criteriaString
    criteria

    Return Value

    A string representation of this instance.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also