Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmField Class / OrderPriority Property


In This Topic
    OrderPriority Property
    In This Topic
    Syntax
    Public Property OrderPriority As System.Short
    public System.short OrderPriority {get; set;}
    public:
    property System.short OrderPriority {
       System.short get();
       void set (    System.short value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also