Configuring Specific OSI PI Collector Fields
Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
The following table outlines the OSI PI Collector-specific configuration fields.
This field... | Indicates... |
---|---|
OSIPI Server | The name of the computer that OSI PI is running on. This should match the server entry in the OSISoft About PI-SDK utility. |
OSIPI User- name | The user name required to connect to the OSI PI Data Archive. PI trusts are not supported and an explicit PI user must be set. |
OSIPI Pass- word | The password required to authenticate with the OSI PI Data Archive. If no password is configured for the OSI PI user, this field can be left blank. |
MaxRecovery Time (hr) | The Maximum Recovery time in hours. See Recovery Mode (OSI PI Collector) for more details. |
Example
The following figure shows the OSI PI Collector configured to collect data from an OSI PI archive on localhost, logging in as the piadmin user. It is also configured for a maximum recovery time of 4 hours.