Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataQuality Interface / IsBad Method


In This Topic
    IsBad Method
    In This Topic
    Whether this instance represents bad data quality.
    Syntax
    Function IsBad() As System.Boolean
    System.bool IsBad()
    System.bool IsBad(); 

    Return Value

    True if bad quality.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also