Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IAlarms Interface / Delete Method


In This Topic
    Delete Method (IAlarms)
    In This Topic
    This provides the functionality to delete or purge Alarms and event from the Alarms and Events database.
    Syntax
    Sub Delete( _
       ByVal backupFileName As System.String, _
       ByVal shouldZipAlarms As System.Boolean, _
       ByVal startTime As System.Date, _
       ByVal endTime As System.Date _
    ) 
    void Delete( 
       System.string backupFileName,
       System.bool shouldZipAlarms,
       System.DateTime startTime,
       System.DateTime endTime
    )
    void Delete( 
       System.String^ backupFileName,
       System.bool shouldZipAlarms,
       System.DateTime startTime,
       System.DateTime endTime
    ) 

    Parameters

    backupFileName
    shouldZipAlarms
    startTime
    endTime
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also