Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Field Class / IsMasterField Property


In This Topic
    IsMasterField Property
    In This Topic
    Identifies the field as a master field.
    Syntax
    Public Property IsMasterField As System.Boolean
    public System.bool IsMasterField {get; set;}
    public:
    property System.bool IsMasterField {
       System.bool get();
       void set (    System.bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also