Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSetState Class / StateHighRawValue Property


In This Topic
    StateHighRawValue Property
    In This Topic
    Raw value less than and equal to this value are in the state.
    Syntax
    Public Property StateHighRawValue As System.Object
    public System.object StateHighRawValue {get; set;}
    public:
    property System.Object^ StateHighRawValue {
       System.Object^ get();
       void set (    System.Object^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also