Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmOpenRecordSetInfo Class / SelectFields Property


In This Topic
    SelectFields Property
    In This Topic
    Syntax
    Public Property SelectFields As AlarmFields
    public AlarmFields SelectFields {get; set;}
    public:
    property AlarmFields^ SelectFields {
       AlarmFields^ get();
       void set (    AlarmFields^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also