Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / TraceVerbose Property


In This Topic
    TraceVerbose Property
    In This Topic
    Gets whether verbose tracing of all messages to file is configured, level set to Verbose.
    Syntax
    Public Shared ReadOnly Property TraceVerbose As System.Boolean
    public static System.bool TraceVerbose {get;}
    public:
    static property System.bool TraceVerbose {
       System.bool get();
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also