Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MessageCriteria Class / Number Property


In This Topic
    Number Property (MessageCriteria)
    In This Topic
    Establish a message number for a query.
    Syntax
    Public Property Number As System.UInteger
    public System.uint Number {get; set;}
    public:
    property System.uint Number {
       System.uint get();
       void set (    System.uint value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also