Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / AddValue Method
A data value.


In This Topic
    AddValue Method (IDataSamples)
    In This Topic
    Append the given data value to this instance.
    Syntax
    Sub AddValue( _
       ByVal value As System.Object _
    ) 
    void AddValue( 
       System.object value
    )
    void AddValue( 
       System.Object^ value
    ) 

    Parameters

    value
    A data value.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also