Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataQuality Interface / IsUncertain Method


In This Topic
    IsUncertain Method
    In This Topic
    Whether this instance represents uncertain data quality.
    Syntax
    Function IsUncertain() As System.Boolean
    System.bool IsUncertain()
    System.bool IsUncertain(); 

    Return Value

    True if uncertain quality.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also