Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / Set Method
A collector to update.


In This Topic
    Set Method (ICollectors)
    In This Topic
    Apply the supplied collector properties to a Historian server. Collectors are uniquely identified by name within a server.
    Syntax
    Sub Set( _
       ByVal collector As Collector _
    ) 
    void Set( 
       Collector collector
    )
    void Set( 
       Collector^ collector
    ) 

    Parameters

    collector
    A collector to update.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also