Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / GetCurrentValue Method
A collector name.
List of collector-specific source addresses.


In This Topic
    GetCurrentValue Method
    In This Topic
    Initiate a request for current values from a collector via a Historian server.
    Syntax
    Sub GetCurrentValue( _
       ByVal collectorname As System.String, _
       ByVal sourceAddresses As System.Collections.Generic.List(Of String) _
    ) 
    void GetCurrentValue( 
       System.string collectorname,
       System.Collections.Generic.List<string> sourceAddresses
    )
    void GetCurrentValue( 
       System.String^ collectorname,
       System.Collections.Generic.List<String^>^ sourceAddresses
    ) 

    Parameters

    collectorname
    A collector name.
    sourceAddresses
    List of collector-specific source addresses.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also