Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianConfiguration Class / MaxDataStores Field


In This Topic
    MaxDataStores Field
    In This Topic
    The maximum number of data stores licensed.
    Syntax
    Public MaxDataStores As System.Long
    public System.long MaxDataStores
    public:
    System.int64 MaxDataStores
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also