Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSetState Class / NumStatesNames Property


In This Topic
    NumStatesNames Property
    In This Topic
    Num names in StateNames list. Only 1 used today.
    Syntax
    Public Property NumStatesNames As System.Integer
    public System.int NumStatesNames {get; set;}
    public:
    property System.int NumStatesNames {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also