Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / SubstatusMask Field


In This Topic
    SubstatusMask Field
    In This Topic
    Bit-mask for extracting quality sub-status.
    Syntax
    Public Const SubstatusMask As System.UInteger
    public const System.uint SubstatusMask
    public:
    const System.uint SubstatusMask
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also