Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / XmlReaderQuotaMaxStringContentLength Property


In This Topic
    XmlReaderQuotaMaxStringContentLength Property
    In This Topic
    Maximum length of a string returned by the reader. Default values is 8K.
    Syntax
    Public Property XmlReaderQuotaMaxStringContentLength As System.Integer
    public System.int XmlReaderQuotaMaxStringContentLength {get; set;}
    public:
    property System.int XmlReaderQuotaMaxStringContentLength {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also