Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / XmlReaderQuotaMaxBytesPerRead Property


In This Topic
    XmlReaderQuotaMaxBytesPerRead Property
    In This Topic
    Maximum bytes consumed by the reader at one time. Default values is 4K.
    Syntax
    Public Property XmlReaderQuotaMaxBytesPerRead As System.Integer
    public System.int XmlReaderQuotaMaxBytesPerRead {get; set;}
    public:
    property System.int XmlReaderQuotaMaxBytesPerRead {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also