Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / XmlReaderQuotaMaxArrayLength Property


In This Topic
    XmlReaderQuotaMaxArrayLength Property
    In This Topic
    Maximum array length returned by the reader. Default value is 1M.
    Syntax
    Public Property XmlReaderQuotaMaxArrayLength As System.Integer
    public System.int XmlReaderQuotaMaxArrayLength {get; set;}
    public:
    property System.int XmlReaderQuotaMaxArrayLength {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also