Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / CloseTimeout Property


In This Topic
    CloseTimeout Property
    In This Topic
    Maximum amount of time to close a connection before timing out. Default value is 1 minute.
    Syntax
    Public Property CloseTimeout As System.TimeSpan
    public System.TimeSpan CloseTimeout {get; set;}
    public:
    property System.TimeSpan CloseTimeout {
       System.TimeSpan get();
       void set (    System.TimeSpan value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also