Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Comment Class / SuppliedUsername Property


In This Topic
    SuppliedUsername Property
    In This Topic
    The user-supplied user name associated with this comment.
    Syntax
    Public Property SuppliedUsername As System.String
    public System.string SuppliedUsername {get; set;}
    public:
    property System.String^ SuppliedUsername {
       System.String^ get();
       void set (    System.String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also