Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / CalculatedQuality Class / Equals Method
An object to test.


In This Topic
    Equals Method (CalculatedQuality)
    In This Topic
    Determines whether this instance is equal to the given object.
    Syntax
    Public Overrides Function Equals( _
       ByVal obj As System.Object _
    ) As System.Boolean
    public override System.bool Equals( 
       System.object obj
    )
    public:
    System.bool Equals( 
       System.Object^ obj
    ) override 

    Parameters

    obj
    An object to test.

    Return Value

    True if the specified object equals this instance.
    Requirements

    Target Platforms: Windows 98, Windows NT 4.0, Windows Millennium Edition, Windows XP Home Edition, Windows XP Professional, Windows Server 2003 family, Windows Vista, Windows Server 2008 family

    See Also