Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmCriteria Class / NumVendorAttributes Property


In This Topic
    NumVendorAttributes Property (AlarmCriteria)
    In This Topic
    NumVendorAttributes
    Syntax
    Public Property NumVendorAttributes As System.Integer
    public System.int NumVendorAttributes {get; set;}
    public:
    property System.int NumVendorAttributes {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also