Ingesting Time Series Data

The Time Series service ingests data using the WebSocket protocol. You may use the Java client library to facilitate ingestion and to avoid setting up a WebSocket, or create your own Websocket connection if you prefer to use a language other than Java.

Ingest with the Java Client Library

After setting up your client, you may create Ingestion Requests using the Ingestion Request Builder. The following shows an example data ingestion request using the Java client. Library.

IngestionRequestBuilder ingestionBuilder = IngestionRequestBuilder.createIngestionRequest()
        .withMessageId("<MessageID>")
        .addIngestionTag(IngestionTag.Builder.createIngestionTag()
            .withTagName("TagName")
            .addDataPoints(
                Arrays.asList(
                            new DataPoint(new Date().getTime(),Math.random(), Quality.GOOD),
                            new DataPoint(new Date().getTime(), "BadValue", Quality.BAD),
                            new DataPoint(new Date().getTime(), null,Quality.UNCERTAIN))
                        )
            .addAttribute("AttributeKey", "AttributeValue")
            .addAttribute("AttributeKey2", "AttributeValue2")
            .build());

String json = ingestionBuilder.build().get(0); 
IngestionResponse response = ClientFactory.ingestionClientForTenant(tenant).ingest(json);
String responseStr = response.getMessageId() + response.getStatusCode();

Ingest with your own WebSocket Connection

You may also setup your own WebSocket in whatever language you prefer. It is recommended you find a WebSocket library in the language you are using to facilitate this process. Once you have a WebSocket library connected, point the request to the endpoint wss://<ingestion_url>. You must also provide the following headers:
  • Authorization: Bearer <token from UAA>
  • Predix-Zone-Id: <your zone id>
  • Origin: http://<your IP address or “localhost”>
An example of a WebSocket implementation for Time Series ingestion is available at https://github.com/PredixDev/timeseries-bootstrap/blob/master/src/main/java/com/ge/predix/solsvc/timeseries/bootstrap/client/TimeseriesClientImpl.java
Note:
The ingestion URI and <Predix-Zone-Id> are included with the environment variables for your application when you bind your application to your Time Series service instance. To view the environment variables, on a command line, enter:
cf env <application_name>

Example Data Ingestion Request

The following shows an example of the JSON payload for an ingestion request:

URL: wss://ingestion_url
Headers:
   Authorization: Bearer <token from trusted issuer>
   Predix-Zone-Id: <Predix-Zone-Id>
   Origin: http://<origin-hostname>/
    
  
Request Payload:
{  
   "messageId": "<MessageID>",
   "body":[  
      {  
         "name":"<TagName>",
         "datapoints":[  
            [  
               <EpochInMs>,
               <Measure>,
               <Quality>
            ]
         ],
         "attributes":{  
            "<AttributeKey>":"<AttributeValue>",
            "<AttributeKey2>":"<AttributeValue2>"
         }
      }
   ]
}

Ingesting backFill data

When ingesting historical or non-live data, it is recommended to use the backFill option to avoid overloading the live data stream. Data ingested using this option will not be available to query immediately.

Note:
This feature is not yet supported in the Java client.

The following JSON is an example of how to use the backFill option.

URL: wss://ingestion_url
Headers:
   Authorization: Bearer <token from trusted issuer>
   Predix-Zone-Id: <Predix-Zone-Id>
   Origin: http://<origin-hostname>/
    
  
Request Payload:
{  
   "messageId": "<MessageID>",
   "body":[  
      {  
         "name":"<TagName>",
         "datapoints":[  
            [  
               <EpochInMs>,
               <Measure>,
               <Quality>
            ]
         ],
         "attributes":{  
            "<AttributeKey>":"<AttributeValue>",
            "<AttributeKey2>":"<AttributeValue2>"
         }
      }
   ],
   "backFill": true
}

Ingestion Nuances

Consider the following when creating an ingestion request:
  • In previous releases, quality was supported as an attribute, but starting with this release,you must explicitly provide quality in each datapoint, along with the timestamp and measurement
  • The Time Series service now accepts compressed (GZIP) JSON payloads. The size limit for the actual JSON payload is 512 KB regardless of the ingestion request format. For compressed payloads, this means that the decompressed payload cannot exceed 512 KB.
  • The <Message Id> can be a string or integer, and must be unique. When using an integer the <MessageID> should be between 0 and 264 (18446744073709551616).
  • The <BackFill> must be a boolean. The ingestion request will return a 400 (Bad Request) status code if the <BackFill> is sent as any other data type. This is an optional parameter, and its value will be false if not specified.

Acknowledgement Message

An acknowledgement message is sent back to the client for each message packet. The following example shows an acknowledgement message:
{
        "messageId": <MessageID>,
        "statusCode": <AcknowledgementStatusCode>
}
The acknowledgement status codes are:
CodeMessage
202Accepted successfully
400Bad request
401Unauthorized
413

Request entity too large

Note: The payload cannot exceed512KB.

503Failed to ingest data

Tips for Data Ingestion

Spread ingestion requests over multiple connections, as sending numerous payloads over the same connection increases wait time for data availability over the query service. Also, be aware of our data plan when using multiple connections.