Overview of the Server-to-Server Distributor
The Historian Server-to-Server distributor is used to send data from a smaller Historian server to a larger, centralized
Historian server. You can then use this data for reporting and analytics. 
You can use either the Server-to-Server collector or the Server-to-Server distributor to send data to a central Historian. However, using the Server-to-Server distributor has the following advantages:
- It simplifies the process of configuring tags at the destination Historian.
- It provides more flexibility at the SCADA level for tag configuration compared to the Server-to-Server collector.
- It allows you to manage tags both from the source and destination Historian servers, whereas the Server-to-Server collector allows you to manage tags only from the destination Historian server.
Features
- You can browse the source for tags and their attributes.
- Only the unsolicited data collection is supported; polled collection is not supported.
- The supported timestamp resolution is 100 milliseconds.
- The collector accepts device timestamps.
- The collector supports data compression.
- Floating point, integer, and string data are supported.
Limitations
- The Server-to-Server distributor forwards only raw data samples, messages, and alarms. It does not perform any calculations on the data.