Accelerating efficiency: How Proplast streamlined planning and boosted accountability with Proficy Scheduler Customer Story Bar Proplast Share Significantly Faster Order Enhanced Visibility and Responsibility Among Employees Streamlined and Efficient Planning Processes Load More Customer Information Introduction Company Proplast Products Proficy Scheduler / ROB-EX, Proficy Industrial Software Proplast is an order-producing company that manufactures extruded hoses, pipes, profiles and non-adhesive tape in plastic. The customers come from industries such as automotive, oil and gas, pharma and wind energy, where high quality and reliable supply has top priority. This means that production planning is a critical factor for Proplast. Now we can deliver an order confirmation in 5 minutes Proplast has achieved great benefits from introducing Proficy Scheduler as a planning tool in the production. Planning used to be made in Excel sheets, on boards and post-it notes but after implementation of Proficy Scheduler big displays have been mounted around the production floor so that everyone can see the current status of the production. An order confirmation which used to be up to 48 hours in the making can now be delivered in five minutes. Visibility makes people feel more responsible Accessible information not only provides a great overview, but it also promotes ownership to the process between employees in the production. COO Stig Bergendorff from Proplast explains:“Our co-workers have been given much more responsibility and ownership because they now can see the plan at all times and see how their work influences on the whole. They report back frequently, 1 to 3 times a day, and then we update the plan so that everybody sees what’s happening right now. The employees now understand the difference they make, encouraging them to take much more responsibility for the production than before.” Faster planning With Proficy Scheduler the planning process at Proplast has become easier, faster and with less friction. It used to be a cumbersome work to process a customer order because the consequences had to be calculated in Excel. Now the planning staff can execute quick and precise analyses in Proficy Scheduler so that the customer can get an almost immediate response.“We have a quality target stating that customers must have order confirmations within 48 hours. If you ask me, we could cut that target to 10 minutes – in fact, we often can confirm in 5 minutes or less,” Stig Bergendorff explains. Acceptance from the production staff Replacing a system can be an unwelcome change for those who are supposed to use it in their daily routine. But the benefits of Proficy Scheduler were immediately so obvious that it went surprisingly smooth.“It was far easier to obtain the acceptance of Proficy Scheduler from the employees than we expected. They had grown used to post-its and printed Excel sheets on a weekly basis on which they could tick off boxes as production went along. But after just a single day, they had accepted that Proficy Scheduler was their new planning tool,” Stig Bergendorff explains. Painless implementation “The actual implementation was easier than expected”, Stig Bergendorff continues. “And much faster. We had a deadline on October the 1st where everything had to be ready. We had completed implementation way earlier than that.”After consulting Proficy Scheduler experts Proplast chose a standard activation. This is a simple and fast activation which means that the customer can begin reaping the benefits of Proficy Scheduler quickly. In fact, it soon became clear that the solution gave much more value than expected.“Before we went live, we had two weeks with the old planning process in Excel, and then we jumped into it. Now we do everything in Proficy Scheduler. We have put up displays and we use the system as planned”, Stig Bergendorff concludes. Even more benefits to come Proficy Scheduler is now an integral part of the daily planning routines at Proplast. The company wants to exploit the system to an even higher degree and is preparing to pull data from purchasing and material handling into the system to optimise the scheduling even more.