Inside Success Story: Early Generator Bearing Vibration Detection at a Combined-Cycle Plant

Author Sticky

Jacqueline Vinyard

Director, Product Marketing

GE Vernova’s Software Business

A professionally trained journalist, Jackie has a degree in journalism and has spent 15+ years’ experience as a researcher and launching innovative technology. She lives in Boulder, CO with her husband, three children and two dogs. Her latest passion is launching software at GE Vernova to accelerate the energy transition and to decarbonize the world.

Feb 24, 2026 Last Updated
3 Minutes Read

A European power generation company serving residential, commercial, and industrial markets uses GE Vernova’s SmartSignal™ predictive analytics to detect early equipment failures across several combined-cycle power plants. They selected SmartSignal along with GE Vernova’s Industrial Managed Services (IMS) to enhance reliability, reduce unplanned downtime, and optimize maintenance operations. Recently, SmartSignal issued an alert to the assigned IMS engineer, signaling a potential issue with a generator bearing.
Prefer to listen?

Stream our audio version

00:00/00:00

What is a generator bearing and why is it critical?

A generator bearing in a combined-cycle plant is a critical mechanical component that supports the generator’s rotor shaft, allowing it to spin smoothly at high speed. The generator converts mechanical energy from the turbine into electrical energy, and its rotor spins at thousands of RPM. Bearings keep the rotor aligned and rotating with minimal friction. Monitoring these components with advanced predictive analytics is essential because:
  • Reliability and Safety: If a bearing fails, the rotor can misalign or seize, causing catastrophic damage to the generator and potentially the turbine.
  • Efficiency: Proper bearing function minimizes friction and vibration, ensuring smooth operation and optimal energy conversion.
  • Cost Impact: Bearing failure can lead to unplanned outages, costing millions in lost generation and repairs.
Using SmartSignal predictive analytics to monitor for early signs of issues, this European utility was able to prevent significant equipment damage and maintain operational reliability.

What Did Our Software Detect?

SmartSignal’s digital twin blueprint, a prebuilt model incorporating known failure modes, flagged a subtle but critical trend: a gradual rise in vibration levels on generator bearing 1. The digital twin continuously compares real-time sensor data against expected behavior, and in this case, it revealed a reading climbing from 60 µm to 71 µm, surpassing the maximum threshold of 68 µm.

This was an early warning of potential bearing distress. Acting on the alert, the IMS team immediately notified the customer’s Center of Excellence (CoE) and recommended a detailed vibration analysis. To ensure proactive follow-up, a formal monitoring case was created, enabling engineers to track the anomaly and prevent escalation.
Generator Bearing Vibration Detected Early at a Combined-Cycle Plant
GE Vernova’s SmartSignal™

Why Do Vibration Trends Matter for Generator Bearings?

Generator bearings operate under extreme conditions, as mentioned above, they support rotors spinning at thousands of RPM. Even small changes in vibration can signal:
  • Lubrication issues or contamination in the oil film.
  • Misalignment or wear in the bearing surface.
  • Imbalance in the rotor, which can escalate into catastrophic failure.
If left unchecked, rising vibration can lead to bearing seizure, rotor damage, and unplanned outages. Predictive analytics helps catch these subtle shifts early, giving operators time to act before damage occurs.

What was the underlying cause?

Following the notification, the site team began closely monitoring the vibrations of the affected bearing and scheduled a comprehensive inspection of both the bearings and the rotor during the next planned outage. During the generator inspection, engineers discovered that several distance pieces within the rotor end winding had loosened. The site team implemented a repair solution to secure the distance pieces.

What was the value to the customer?

Thanks to the early notification from GE Vernova’s IMS team, the customer was able to proactively prepare for an extended inspection of the generator and ultimately identify the root cause of the developing issue.

In the worst-case scenario, complete loosening of the distance pieces could have damaged the end winding, potentially necessitating a full rotor replacement. Following the generator restart after the outage, both the customer and the IMS teams confirmed that the corrective actions were effective, as vibration levels stabilized and subsequently decreased to the values predicted by the model. The customer estimated that approximately $3,800,000* in costs were avoided.

*Avoided costs are based on North American average production loss

Author Section

Author

Jacqueline Vinyard

Director, Product Marketing
GE Vernova’s Software Business

A professionally trained journalist, Jackie has a degree in journalism and has spent 15+ years’ experience as a researcher and launching innovative technology. She lives in Boulder, CO with her husband, three children and two dogs. Her latest passion is launching software at GE Vernova to accelerate the energy transition and to decarbonize the world.