From Fragmented Systems to One Coordinated Transmission Grid

Author Sticky

Nitesh Kumar Kaveti

Product Marketing Manager

Grid Software, GE Vernova

Nitesh Kumar Kaveti is the Product Marketing Manager for Grid Software at GE Vernova, where he leads global go-to-market strategy for the Transmission product suite. His work focuses on helping utilities unlock greater value through technology and navigate their path toward grid modernization. With close to two decades of experience in product marketing, he has led global go-to-market strategies that drive growth and transformation. Holds a Master of Business in Global Business Analysis from Manchester Business School (UK) with a strong foundation in technology, systems thinking, and problem-solving

Jun 09, 2026 Last Updated
3 Minutes read

Why traditional transmission operating models no longer scale

The current operating model of transmission systems has reached its breaking point. It will not scale to support the level of speed, interdependence, and variability that now defines the grid. Utilities can no longer rely on loosely connected systems and sequential decision-making to manage increasingly dynamic conditions.

Transmission systems were initially managed through a relatively cohesive operational setup because the grid itself was simpler. Power flows were predictable, generation was largely controllable, and system conditions evolved within a stable range.

As the grid expanded and new constraints emerged, utilities responded pragmatically by introducing systems to solve specific problems, to EMS- like planning tools, stability monitoring systems, forecasting tools, asset systems etc., Each system was designed to address a clearly defined operational need.

Over time, this led to an operating environment where the transmission grid was managed through a system of systems. Operators could move across systems, interpret outputs, validate conditions, and then act. Decisions were made sequentially, and the time required to reconcile information across systems did not materially affect outcomes.

Today’s grid is more dynamic, interconnected, and time-sensitive. Electrification has introduced new and often non-linear demand patterns, with significant load growth in localized pockets such as data centers and industrial clusters. Renewable generation has shifted the grid to a state that is inherently variable and weather-dependent. Power flows are no longer stable or unidirectional; they shift based on generation availability, demand patterns, and network constraints. At the same time, extreme weather events have become more frequent.

Infrastructure expansion has not kept pace with these changes, increasing reliance on operational measures to manage constraints. Compounding all of this is a workforce transition, where experienced operators are retiring, and institutional knowledge is becoming harder to replace.

In this environment, the sequential decision process of moving across systems to build a complete picture before acting introduces delay. That delay is operationally visible, and it shows up as conservative operating limits, delayed responses to emerging instability, inefficient congestion management, and missed opportunities to utilize available capacity. The issue is no longer whether each system is capable; most are highly capable within their domains. The issue is that they are not coordinated in time.

This is why the current operating model has reached its breaking point.

Introducing GridOS® for Transmission by GE Vernova

gridos-for-transmission
To address the limits of the current operating model, GE Vernova is introducing GridOS for Transmission, a single coordinated operational solution designed for how modern transmission grids function in the real world.

GridOS for Transmission is not an incremental enhancement to existing systems, and it is not another application added to the stack. It is a unified operational environment that brings together real-time operations, transmission capacity, system stability, and forward-looking conditions into a single, continuously aligned decision system. Its purpose is to remove the fragmentation across systems so that operators no longer have to assemble context before acting. Instead, it allows utilities to operate these systems on a shared, time-synchronized view of the grid where insight, decision, and action are aligned.

This “unification layer” is fundamental to day-to-day operations. Firstly, it allows managing real-time system state, network topology, and control actions within one consistent operational context.

With GridOS for Transmission, the capacity is continuously updated based on actual operating conditions and forecast inputs, thus, no longer treated as static. Further, stability is not monitored separately, but understood as part of the same operational picture that informs decisions. Additionally, the unified environment allows embedding forecasts into the decision environment before constraints materialize.

Underlying all of this is a shared data and model foundation, ensuring that every application operates on a consistent representation of the network, eliminating the need for cross-system reconciliation.

GridOS for Transmission is designed to be adopted at a three-level progressive operating framework, recognizing that utilities are at different stages of maturity.

Level 1:
Reliable & Resilient Grid

  • At the first level, transmission utilities establish the core capabilities required to operate the grid safely, reliably, and with confidence.
  • GridOS for Transmission brings together foundational applications that provide real-time visibility, monitoring, and control of the network. These capabilities create a unified operational environment where data is consistent, systems are connected, and operators have a clear and accurate view of grid conditions.
Core capabilities include:
  • Real-time grid monitoring and control through AEMS
  • A unified, governed data foundation with Data Fabric & Connect
  • Accurate network modeling and system visibility
  • Dynamic awareness of line capacity using real-time and forecast-based DDLR
  • Baseline system visibility through WAMS
  • Short-term forecasting to support operational readiness
Utilities can further extend this foundation with additional capabilities that enhance visibility beyond the control room, including visual intelligence, geospatial network modeling, field assessment, and disruption preparedness.

The outcome of Level 1 is a trusted operational foundation, ensuring utilities have the visibility, control, and data consistency needed to operate the grid reliably today while preparing for future complexity.

Level 2:
Optimized Grid

This level includes all Level 1 capabilities, while introducing advanced operational intelligence that enables operators to move from monitoring the grid to actively optimizing it in real time.

At this stage, GridOS for Transmission enhances the AEMS with advanced visibility, operator decision support, and system calibration capabilities, enabling faster and more accurate decision-making. Optimization functions such as optimal power flow, VAR dispatch, and transmission switching allow operators to improve network performance and reduce congestion.

Deeper visibility into system behavior is also introduced through WAMS, including oscillation monitoring, system strength analysis, and islanding and resynchronization insights helping operators understand how the grid behaves under dynamic conditions.

Utilities can further extend operational intelligence through asset and risk awareness capabilities such as field assessment and disruption preparedness, while early-stage DER orchestration enables initial coordination of distributed energy resources. The result is a more efficient transmission network where utilities can better understand available capacity, respond faster to changing conditions, and make more informed operational decisions.

Level 3:
Intelligent Grid

Level 3 represents a fully evolved stage of transmission operations where utilities move beyond optimization to coordinated, system-wide intelligence.

This level includes all capabilities from Level 1 and Level 2, while introducing advanced capabilities that enable the grid to be operated as a unified and responsive system.

At this stage, GridOS for Transmission brings together advanced AEMS capabilities, system restoration functions, and comprehensive WAMS integration to provide continuous visibility into system dynamics. Utilities gain deeper insights into inertia, disturbances, contingencies, and system behavior, enabling proactive management of stability and risk.

Additional capabilities extend coordination beyond core operations, including integration with markets, generation optimization, and advanced DER orchestration aligning decisions across the broader energy ecosystem.
As operational maturity increases, utilities can also leverage advanced analytics, model validation, and system intelligence capabilities to continuously improve grid performance and reliability.

The result is a transmission system that is not only visible and optimized, but intelligently coordinated, capable of maintaining stability, responding to disruptions, and operating efficiently under highly dynamic conditions.

What utilities become and what changes in practice

The impact of GridOS for Transmission is not in the systems it connects, but in how it changes the way the grid is operated. As utilities move to a coordinated operating model, they build critical competencies that were difficult to achieve in a fragmented environment. These include continuous network awareness, where operators rely on a single, consistent view of the grid; dynamic capacity management, where transmission limits reflect actual conditions rather than static assumptions; proactive stability management, where system behavior is understood early enough to influence outcomes; and coordinated response, where actions are taken with full system context rather than in isolation. Together, these capabilities enable utilities to operate the grid with greater precision, confidence, and control.

At the operator level, instead of switching between systems, validating differences, and assembling context under time pressure, operators work from a unified operational view. The role shifts from managing systems to managing the grid itself, with clarity and speed.

At the utility level, this entails utilizing existing transmission capacity more effectively, reducing congestion and curtailment, responding faster to emerging risks, and operating a more complex grid without a proportional increase in operational burden.

The result is improved efficiency and a fundamentally stronger and more resilient transmission system.

The new phase of transmission operations

gridos-for-transmission
A fundamental shift is a necessity for modernizing grid operations today, and this change must happen through aligning the existing capabilities to coordinate system-wide insights, decisions, and actions.

GridOS for Transmission is designed for this shift. It enables utilities to move from fragmented decision-making to coordinated operations at a pace aligned with the utility maturity, while unlocking the full potential of the infrastructure they already have.

The new phase of transmission performance will not be defined by how much new capacity is built, but by how effectively the existing grid is understood, utilized, and operated in real time.

To learn more about the announcement, read the full press release here.

Author Section

Author

Nitesh Kumar Kaveti

Product Marketing Manager
Grid Software, GE Vernova

Nitesh Kumar Kaveti is the Product Marketing Manager for Grid Software at GE Vernova, where he leads global go-to-market strategy for the Transmission product suite. His work focuses on helping utilities unlock greater value through technology and navigate their path toward grid modernization. With close to two decades of experience in product marketing, he has led global go-to-market strategies that drive growth and transformation. Holds a Master of Business in Global Business Analysis from Manchester Business School (UK) with a strong foundation in technology, systems thinking, and problem-solving