DDLR and Energy Management System: Unlocking Grid Capacity and Control

Author Sticky

Chris Heschmeyer

Principal Solutions Architect- Transmission & Market Management Systems Solutions

Grid Software, GE Vernova

Chris Heschmeyer has spent the last 6 years as a Principal Solutions Architect for Transmission and Market Management Systems Solutions at GE Vernova.  Prior to this, he spent 20 years in various roles in the Transmission Organization of an 18,000 MW electric utility in the Midwest.  For 15 of those years, he managed the real-time operations and staff of the Transmission Control Center, followed by 3 years managing the EMS support group.  He held a NERC System Operator/Reliability Coordinator certification from 2003 until 2023.

Jun 08, 2026 Last Updated
3 Minutes read

Grid challenges across decisions and capacity

Power transmission operations today are under increasing pressure. Renewable variability, changing load patterns, and tighter operating margins are making the system more dynamic than ever. Utilities are expected to respond faster, operate more efficiently, and still maintain absolute reliability with virtually no power grid disruption at all.

In this environment, two distinct challenges are becoming more visible.

The first emerges when advanced energy systems, like EMS, lack advanced grid software. Without capabilities such as grid analytics, real-time contingency analysis, intelligent alarm processing, or restoration support, operators are forced into reactive decision-making. Situational awareness is fragmented; response times are slower, and actions are often more extreme than necessary, especially during stressed conditions.

The second challenge appears even in utilities with strong operational systems. Many still rely on static or seasonal ratings to define how much power the grid can carry. These limits are intentionally conservative, but they do not reflect real-time conditions. As a result, available capacity remains unused; congestion appears earlier than necessary, and renewables generation is curtailed despite favorable conditions.

These are two different problems, but both directly impact how effectively the grid is operated.

Advanced EMS transforms grid operations

Modern Advanced Energy Systems (AEMS) platforms address the first problem by fundamentally improving how decisions are made.

With advanced applications and powerful energy data management systems, operators gain a unified and real-time view of the system, supported by faster analysis and more intelligent guidance. Contingencies can be evaluated quickly; alarms are prioritized and contextualized, and restoration strategies can be executed with greater coordination and confidence.

Upgrading to the latest AEMS is not just a technical refresh; it is an operational upgrade. It enables control rooms to move from reactive response to proactive decision-making, especially under complex and evolving grid conditions.

However, even with these advancements, one limitation remains.

All decisions are still executed within predefined system limits, that are often based on static assumptions rather than real-world conditions.
Advanced EMS transforms grid operations

GridOS DDLR unlocks real-time capacity

To address this second challenge, utilities need visibility into system capacity as it exists in real time, which can only come from truly smart grid software. GridOS DDLR provides that capability.

DDLR continuously evaluates environmental conditions such as ambient temperature, wind speed, and direction, along with conductor characteristics, to determine real-time and forecasted operating limits. This replaces static assumptions with dynamic, condition-based ratings revealing how much the grid can safely carry at any given moment.

This has an immediate impact across the organization. Operators gain flexibility, enabling them to potentially run the system closer to actual limits as needed while still conforming to their company’s official ratings policies.. Planning teams can distinguish between true constraints and conservative assumptions, enabling better investment decisions. Asset teams gain clearer insight into how infrastructure is actually performing, helping prioritize upgrades more effectively. And offline study modes help system planners and ops planners with their core job functions while the control center gets the benefits of higher-performing physical network assets.

Equally important is how DDLR gets deployed. As asensor-free, SaaS utilities software application, it can be implemented quickly and scaled across the network. It operates independently of EMS upgrade timelines, allowing utilities to begin unlocking capacity immediately through an IT-led approach.

DDLR is configured to match a utility’s existing ratings methodology, but is updated at a high geospatial and temporal resolution in real-time and as a forecast. There is no “black box magic” simply producing higher numbers – NERC FAC-008 conformance and evidence gathering are part of its feature set. DDLR is not just for lines, it also incorporates all of the various terminal equipment found in the substation such as busbar, switches, wave traps, etc. Therefore, DDLR is a true facilities ratings management system for usage across many departments within the utility.

AEMS and DDLR working together

AEMS and DDLR working together
The real value emerges when AEMS and GridOS DDLR operate together as part of a coordinated workflow.

AEMS continuously monitors the grid, analyzes system conditions, and identifies emerging constraints or risks. When a transmission corridor approaches its limit, AEMS can trigger a request for updated capacity.

GridOS DDLR then evaluates real-time environmental and asset conditions to calculate the actual safe operating limit for that corridor. These updated limits are fed back into AEMS as operational inputs.

AEMS uses these dynamic limits within its analytical and decision-making applications—re-running power flow, contingency analysis, and optimization based on the updated capacity. Operators can then execute decisions that reflect the true capability of the system, not static assumptions.

This creates a closed operational loop where system visibility, capacity evaluation, and decision execution continuously inform each other.

Operating closer to true capacity

Modern grid operations require both stronger decision-making and a more accurate understanding of system capacity.

Advanced EMS brings the intelligence needed to make better decisions. DDLR ensures those decisions are based on real-world limits. Together, they allow utilities to operate the grid with greater precision, flexibility, and confidence.

As the grid continues to evolve, aligning decisions with actual system capability is becoming essential not just for efficiency, but for reliably managing the complexity of the modern power system.

For more information on GridOS DDLR, check out our solution paper on the subject.

Author Section

Author

Chris Heschmeyer

Principal Solutions Architect- Transmission & Market Management Systems Solutions
Grid Software, GE Vernova

Chris Heschmeyer has spent the last 6 years as a Principal Solutions Architect for Transmission and Market Management Systems Solutions at GE Vernova.  Prior to this, he spent 20 years in various roles in the Transmission Organization of an 18,000 MW electric utility in the Midwest.  For 15 of those years, he managed the real-time operations and staff of the Transmission Control Center, followed by 3 years managing the EMS support group.  He held a NERC System Operator/Reliability Coordinator certification from 2003 until 2023.