Capacity Intelligence: Unlocking the True Potential of Transmission Networks

Author Sticky

Nitesh Kumar Kaveti

Product Marketing Manager

Grid Software, GE Vernova

Nitesh Kumar Kaveti is the Product Marketing Manager for Grid Software at GE Vernova, where he leads global go-to-market strategy for the Transmission product suite. His work focuses on helping utilities unlock greater value through technology and navigate their path toward grid modernization. With close to two decades of experience in product marketing, he has led global go-to-market strategies that drive growth and transformation. Holds a Master of Business in Global Business Analysis from Manchester Business School (UK) with a strong foundation in technology, systems thinking, and problem-solving

Jul 23, 2026 Last Updated
3 minutes read

Grid capacity constraints

As demand for power continues to skyrocket, many utilities find themselves struggling to keep up with transmission capacity. As the link between large-scale generation resources and the distribution grid, transmission utilities in particular find themselves under scrutiny when grid capacity constraints and transmission congestion occur. More often than not, they conclude that their networks are running out of capacity.

But in many cases, that isn’t true. The real constraint is not how much capacity exists, but how much is visible and can be trusted in real time.
GE Vernova

What capacity challenges do transmission utilities face?

Transmission systems today are operating in conditions they were not originally designed for. For example, renewables generation is scaling rapidly and introduces immense variability in power flows from weather-dependent generation patterns. Intermittent shift in power flow and changing conditions, potentially by the hour, can tremendously affect predictability; and power that appears stable at one moment may look completely different the next.

At the same time, demand is soaring, —driven by electrification, industrial growth, and new load sources such as data centers.

According to the International Energy Agency, global electricity demand is forecast to grow close to 4% annually through 2027—one of the fastest sustained growth rates in recent years.

And then there’s the other, physical side of the problem; the process of expanding transmission infrastructure is frustratingly slow. In many regions, it takes years, sometimes over a decade, to plan, approve, and build new lines. From permitting, to regulatory compliance, to securing capital and beyond, everything takes time.

Transmission utilities are caught in an untenable position: the grid is being strained to its limits, but the ability to expand it is not keeping pace.

What do transmission capacity challenges look like behind the scenes?

Consider the example of a high renewables generation period where wind is strong, solar is peaking, and overall power flows are increasing across key corridors. Congestion alerts begin to appear, and now the operator has to decide whether to push more power or hold back.

On paper, it is a simple, this-or-that decision. In reality, it’s anything but! The true question is not just how much load is on the lines — it’s really how much of said load the line can safely carry.

That’s where the problem starts. The transmission capacity measurements visible to the control-room operator are static limits based on conservative assumptions, often reflecting worst-case conditions rather than what is happening in real time.

The result? The operator takes a conservative approach. Generation is curtailed and margin is preserved. Few people will question the logic of this safe, conservative decision, not realizing that the line could in fact have carried more power. More power would have been delivered, and the curtailment may have been minimized or even avoided altogether. But this didn’t happen in the above scenario—not because the capacity didn’t exist, but because it wasn’t visible enough to be confirmed .

This lack of visibility and confidence happens disturbingly often, and across many divisions in the average utility organization. Planning teams, for example, must frequently rely on roughly averaged or seasonal assumptions. Asset teams may have to assume the presence of thermal stress rather than confirming it visually. And Finance teams must often make investment decisions based on what the network appears to be able to handle — not necessarily what it genuinely can.

Such lack of confidence, accuracy, and precision in decision making means that transmission utilities frequently underutilize existing infrastructure, overestimate congestion, and waste precious capital on unnecessary new construction.
GE Vernova

How can utilities optimize transmission capacity?

To properly and accurately assess congestion and capacity, operators and planners need to analyze their data and answer four simple questions:
  • What can the system safely handle right now?
  • How is that going to change over the next few hours?
  • What happens if conditions shift (wind decreases, temperature jumps, etc.)?
  • How confidently can decisions be made based on the assessments?
All of those questions can be answered by rethinking capacity. Instead of treating capacity as a fixed limit, it should be thought of as dynamic and variable. In other words, something that changes continuously along with environmental conditions. That happens by adopting capacity intelligence.

What is transmission capacity intelligence?

Capacity intelligence is the ability to continuously understand, anticipate, and apply true transmission capacity based on real-world conditions.

It’s a combination of:

GE Vernova GridOS® Digital Dynamic Line Rating (DDLR) unlocks true capacity intelligence.

GridOS DDLR unites weather data, conductor characteristics, and system conditions to continuously determine safe transmission limits, both in real time and look ahead, and embeds key insights into operator workflow.

It is a software-based approach to dynamic line rating, without the costly line sensors of its hardware-based antithesis.

Readily scalable and user-friendly, GridOS DDLR closes the gap between how capacity is defined and used . Its software-based approach uses weather data, physics-based models, and system-wide inputs to estimate capacity across the network, enabling broader coverage and scalability without extensive field infrastructure

How does capacity intelligence increase transmission reliability?

Once a utility unlocks capacity intelligence, the shift is rapid.

Operators, planners, and asset management teams no longer need to rely on conservative, imprecise limits. They can make decisions with more confidence based on the precisely calculated capacity, leading to greater efficiency and cost optimizations for the utility and better service for customers. Everyone wins.

Instead of treating capacity constraints purely as physical limitations, utilities can address them as visibility and confidence challenges, unlocking existing capacity before committing to long-cycle infrastructure investments.

For more information on unlocking transmission capacity, read our solution paper on GridOS® Digital Dynamic Line Rating (DDLR).

Author Section

Author

Nitesh Kumar Kaveti

Product Marketing Manager
Grid Software, GE Vernova

Nitesh Kumar Kaveti is the Product Marketing Manager for Grid Software at GE Vernova, where he leads global go-to-market strategy for the Transmission product suite. His work focuses on helping utilities unlock greater value through technology and navigate their path toward grid modernization. With close to two decades of experience in product marketing, he has led global go-to-market strategies that drive growth and transformation. Holds a Master of Business in Global Business Analysis from Manchester Business School (UK) with a strong foundation in technology, systems thinking, and problem-solving