; Default Configuration Script for MDS iNET-II 900, version 2.7.0 ; IP Address: 192.168.1.1 ;The IPv4 address of this unit. This field is unnecessary if DHCP is enabled. Caution!!! Changing this value via the network will cause a loss of communication. IP Netmask: 255.255.0.0 ;The IPv4 local subnet mask. This field is unnecessary if DHCP is enabled. IP Gateway: 0.0.0.0 ;The IPv4 address of the network gateway device, typically a router. This field is unnecessary if DHCP is enabled. Model Number: 900 ;(RO) The model number of this unit. This value is set by the factory and cannot be changed. DHCP Client: disabled ;Dynamic Host Configuration Protocol Client. When enabled, the IP address, netmask and gateway will be automatically configured. Note that a device running as a DHCP server must be present on the local network to fulfill the DHCP request and powerup. Unit Name: ;A name for this unit. It appears at the top of every menu screen. Owner: ;The name of the owner of this unit. Contact: ;The contact person regarding this unit. Description: ;A brief general description of this unit. Location: ;The location of this unit. Com1 Byte Format: 8N1 ;Configuration of character size, type of parity, and number of stop bits to be used. Com2 Byte Format: 8N1 ;Configuration of character size, type of parity, and number of stop bits to be used. Max Remotes Allowed: 50 ;The maximum number of remotes allowed to connect to this Access Point. Device Mode: Remote ;Configures the unit to act as a Remote or an Access Point . The Access Point option is not allowed unless the unit is specifically ordered as such, or an authorization key has been purchased to allow it. Dwell Time: 32.8 ;The amount of time the unit spends at any given frequency in its hopping pattern. This field is only changable by a Master. Remotes read the Masters value upon association. Hop Pattern: 1 ;A seed used to create the pseudo-random hopping pattern Lan Enable: enabled ;Enable or Disable the Ethernet LAN port. Network Name: Not Programmed ;The name of the network this unit belongs to. The unit will only communicate with devices having identical network names. Date Format: Generic ;Specifies the format of the date. Generic=dd Mmm yyyy. European=dd-mm-yyyy. US=mm-dd-yyyy. Console Baud: 19200 ;The baud rate of the serial menu console. Default value is 19200 bps. Company Name: MDS ;(RO) The name of the product manufacturer. Version Name: 06-6110A01 ;(RO) The software part number. Product Name: iNET-II ;(RO) The name of this device Beacon Period: Normal ;The amount of time in milliseconds between beacon transmissions by the AP Data Rate: 512kbps ;The selected over-the-air data rate. A lower data rate generally allows more distance between the unit and its Master. Association Events: disabled ;Enable/Disable Association Events RF Output Power Setpoint: 30 ;The desired amount of RF output power, measured in dBm. Skipped Hop Zone1: Active ;The configured RF zones to skip Skipped Hop Zone2: Active ;The configured RF zones to skip Skipped Hop Zone3: Active ;The configured RF zones to skip Skipped Hop Zone4: Active ;The configured RF zones to skip Skipped Hop Zone5: Active ;The configured RF zones to skip Skipped Hop Zone6: Active ;The configured RF zones to skip Skipped Hop Zone7: Active ;The configured RF zones to skip Skipped Hop Zone8: Active ;The configured RF zones to skip Skipped Hop Zone9: Active ;The configured RF zones to skip Skipped Hop Zone10: Active ;The configured RF zones to skip Firmware TFTP Host IP: 127.0.0.1 ;IP Address of the TFTP Host from which firmware images are downloaded Firmware TFTP Filename: ;File name on the TFTP Host of the firmware image to download Eventlog TFTP Host IP: 127.0.0.1 ;IP Address of TFTP Host to which to send the event log Eventlog TFTP Filename: ;File name on the TFTP Host of the event log Config Script TFTP Host IP: 127.0.0.1 ;TFTP Host to which configuration scripts will be sent and received. Config Script TFTP Filename: ;File name of the configuration script. Fragmentation Threshold: 1600 ;Max packet size allowed before fragmentation occurs RTS Threshold: 500 ;Number of bytes for the RTS/CTS handshake boundary RSSI Threshold: -90 ;RSSI value at which the connection is deemed 'degraded' SNR Threshold: 0 ;SNR value at which the connection is deemed 'degraded' SNMP Read Community: public ;Community string for read access using SNMPv1 SNMP Write Community: private ;Community string for write access using SNMPv1 SNMP Trap Community: public ;Community string sent with traps using SNMPv1 SNMP Trap Manager #1: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent SNMP Trap Manager #2: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent SNMP Trap Manager #3: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent SNMP Trap Manager #4: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent Auth trap enable: disabled ;Setting to enable SNMP authentication traps Trap Version: v1 Traps ;Selects which SNMP trap format to send TFTP Timeout: 10 ;Timeout, in seconds, for TFTP file transfers Remote Database Timeout: 5 ;Timeout, in minutes, for ageing Remotes and Endpoints out of the Remote Database Com1 Serial Data Enable: disabled ;Setting to enable COM1 data mode Com1 Serial Data Baud Rate: 9600 ;Baud rate for COM1 data mode Com1 Serial Data Remote IP Address: 0.0.0.0 ;COM1 data will be sent to this IP address Com1 Serial Data Remote IP Port: 30010 ;COM1 data will be sent to this IP port Com1 Serial Data Local IP Port: 30010 ;COM1 data will be received on this IP port Com2 Serial Data Enable: enabled ;Setting to enable COM2 data mode Com2 Serial Data Baud Rate: 9600 ;Baud rate for COM2 data mode Com2 Serial Data Remote IP Address: 0.0.0.0 ;COM2 data will be sent to this IP address Com2 Serial Data Remote IP Port: 30011 ;COM2 data will be sent to this IP port Com2 Serial Data Local IP Port: 30011 ;COM2 data will be received on this IP port Com2 Serial Data Flow Control: disabled ;Setting to enable hardware flow control (RTS/CTS) in COM2 data mode SNTP Server IP: 0.0.0.0 ;The IPv4 address of NTP/SNTP Time Server Com1 Serial Data Seamless Mode: disabled ;Setting to enable seamless mode for COM1 data mode Com2 Serial Data Seamless Mode: disabled ;Setting to enable seamless mode for COM2 data mode Com1 Serial Data Delimiter Chars: 4 ;Minimum number of characters which will be considered a gap in seamless mode for COM1 Com2 Serial Data Delimiter Chars: 4 ;Minimum number of characters which will be considered a gap in seamless mode for COM2 Com1 Serial Data Buffer Size: 64 ;Number of output characters which will be buffered in seamless mode for COM1 Com2 Serial Data Buffer Size: 64 ;Number of output characters which will be buffered in seamless mode for COM2 SNMP Mode: SNMP_V1V2V3 ;Set SNMP Agent Operating Mode DHCPd Server Enable: disabled ;Enable/Disable DHCP Server Daemon DHCPd Netmask: 0.0.0.0 ;The IP Address to be used as the DHCP Netmask DHCPd Start Address: 0.0.0.0 ;The IP Address to be used as the starting address DHCPd End Address: 0.0.0.0 ;The IP Address to be used as the ending address DHCPd DNS Address: 0.0.0.0 ;The IP Address to be used as the DNS Address DHCPd WINS Address: 0.0.0.0 ;The IP Address to be used as the WINS Address Encryption Enable: disabled ;Setting to enable over-the-air data encryption Telnet Enable: enabled ;Setting to enable the Telnet interface HTTP MD5 Authentication: disabled ;Setting to enable MD5 Digest Authentication Automatic Key Rotation: enabled ;Setting to enable Automatic Key Rotation Watch-Link-Status Flag @ AP: disabled ;A flag that controls whether the Remotes care about the AP's Ethernet Link Status Syslog Server Address: 0.0.0.0 ;The IPv4 address of a syslog server Ethernet Rate Limit: 500000 ;Ethernet traffic rate limit on Ethernet Port. (used for monitoring) Com1 Serial Data Multicast IP Port: 30010 ;COM1 data will be sent/recieved to this IP port, depending on data mode Com2 Serial Data Multicast IP Port: 30011 ;COM2 data will be sent/recieved to this IP port, depending on data mode Com1 Serial Data Primary TCP Client IP Address: 0.0.0.0 ;COM1 data will be sent to this IP address Com1 Serial Data Primary TCP Client IP Port: 30010 ;COM1 data will be sent to this IP port Com1 Serial Data Secondary TCP Client IP Port: 30010 ;COM1 data will be sent to this IP port Com1 Serial Data Secondary TCP Client IP Address: 0.0.0.0 ;COM1 data will be sent to this IP address Com2 Serial Data Primary TCP Client IP Address: 0.0.0.0 ;COM2 data will be sent to this IP address Com2 Serial Data Primary TCP Client IP Port: 30011 ;COM2 data will be sent to this IP port Com2 Serial Data Secondary TCP Client IP Port: 30011 ;COM2 data will be sent to this IP port Com2 Serial Data Secondary TCP Client IP Address: 0.0.0.0 ;COM2 data will be sent to this IP address Com1 Serial Data TCP Outgoing Keepalive: 5 ;Com1 TCP connection will be reset after this period of inactivity Com2 Serial Data TCP Outgoing Keepalive: 5 ;Com2 TCP connection will be reset after this period of inactivity Com1 Serial Data TTL: 1 ;Com1 TCP Time-To-Live Value Com2 Serial Data TTL: 1 ;Com2 TCP Time-To-Live Value Com1 Serial Data PPP Address: 0.0.0.0 ;Com1 IP address for connected PPP device Com2 Serial Data PPP Address: 0.0.0.0 ;Com2 IP address for connected PPP device Com1 Serial Data Multi Packet Sends: 6 ;Com1 redundant UDP packet sends Com2 Serial Data Multi Packet Sends: 6 ;Com2 redundant UDP packet sends Snmp v3 password mode: MANAGER ;Snmp v3 password mode Snmp v3 auth password: MDSAuthPwd ;Snmp v3 auth password Snmp v3 priv password: MDSPrivPwd ;Snmp v3 priv password AP Automatic Remote Upgrade Feature: disabled ;AP Automatic Remote Upgrade Feature AP Reboot mode for Remotes: disabled ;Tells Remote whether to reboot or not after upgrade Poll Address: 0.0.0.0 ;The IP Address to be polled for link status Compress Enable: disabled ;Enable/Disable compression of frames over the air. Com1 UDP Packet Repeat Mode: disabled ;Com1 Turns on Packet Transmittion and Reception of Multiple UDP Packets Com2 UDP Packet Repeat Mode: disabled ;Com2 Turns on Packet Transmittion and Reception of Multiple UDP Packets Com1 Serial Data TCP Incoming Keepalive: 600 ;Com1 TCP connection will be reset after this period of inactivity Com2 Serial Data TCP Incoming Keepalive: 600 ;Com2 TCP connection will be reset after this period of inactivity Com1 Serial Data Multicast Address: 224.0.0.0 ;COM1 data will be sent/received on this IP address, depending on data mode Com2 Serial Data Multicast Address: 224.0.0.0 ;COM2 data will be sent/received on this IP address, depending on data mode Com1 Serial Data IP Mode: UDP_P2P ;IP Protocol for COM1 data mode Com2 Serial Data IP Mode: UDP_P2P ;IP Protocol for COM2 data mode UTC Time Offset: 0 ;Difference between yout time and UTC time. Redundant Events: FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF ;Redundant Events Bit Array Loss of Association Timeout: 1200 ;Redundancy switch over after Lack of Association Timeout Lack of Associated Remotes Timeout: 1200 ;Redundancy switch over after Lack of Associated Remotes Timeout Maximum Retry Errors: 300 ;Redundancy switch over after Maximum Retry Errors Retry Error Time Interval: 300 ;Time Interval to log Retry Errors Maximum Receive Errors: 300 ;Redundancy switch over after Maximum Receive Errors Receive Error Time Interval: 300 ;Time Interval to log Receive Errors Target IP Address Route for channel 0: ;Target IP Address Route for the messages sent to the channel 0 by the DF1/EIP component. Target IP Address Route for channel 1: ;Target IP Address Route for the messages sent to the channel 1 by the DF1/EIP component. Target IP Address Route for channel 2: ;Target IP Address Route for the messages sent to the channel 2 by the DF1/EIP component. Target IP Address Route for channel 3: ;Target IP Address Route for the messages sent to the channel 3 by the DF1/EIP component. Target IP Address Route for channel 4: ;Target IP Address Route for the messages sent to the channel 4 by the DF1/EIP component. Target IP Address Route for channel 5: ;Target IP Address Route for the messages sent to the channel 5 by the DF1/EIP component. Target IP Address Route for channel 6: ;Target IP Address Route for the messages sent to the channel 6 by the DF1/EIP component. Target IP Address Route for channel 7: ;Target IP Address Route for the messages sent to the channel 7 by the DF1/EIP component. Target IP Address Route for channel 8: ;Target IP Address Route for the messages sent to the channel 8 by the DF1/EIP component. Target IP Address Route for channel 9: ;Target IP Address Route for the messages sent to the channel 9 by the DF1/EIP component. Target IP Address Route for channel 10: ;Target IP Address Route for the messages sent to the channel 10 by the DF1/EIP component. Target IP Address Route for channel 11: ;Target IP Address Route for the messages sent to the channel 11 by the DF1/EIP component. Target IP Address Route for channel 12: ;Target IP Address Route for the messages sent to the channel 12 by the DF1/EIP component. Target IP Address Route for channel 13: ;Target IP Address Route for the messages sent to the channel 13 by the DF1/EIP component. Target IP Address Route for channel 14: ;Target IP Address Route for the messages sent to the channel 14 by the DF1/EIP component. Target IP Address Route for channel 15: ;Target IP Address Route for the messages sent to the channel 15 by the DF1/EIP component. Target IP Address Route for channel 16: ;Target IP Address Route for the messages sent to the channel 16 by the DF1/EIP component. Target IP Address Route for channel 17: ;Target IP Address Route for the messages sent to the channel 17 by the DF1/EIP component. Target IP Address Route for channel 18: ;Target IP Address Route for the messages sent to the channel 18 by the DF1/EIP component. Target IP Address Route for channel 19: ;Target IP Address Route for the messages sent to the channel 19 by the DF1/EIP component. Target IP Address Route for channel 20: ;Target IP Address Route for the messages sent to the channel 20 by the DF1/EIP component. Target IP Address Route for channel 21: ;Target IP Address Route for the messages sent to the channel 21 by the DF1/EIP component. Target IP Address Route for channel 22: ;Target IP Address Route for the messages sent to the channel 22 by the DF1/EIP component. Target IP Address Route for channel 23: ;Target IP Address Route for the messages sent to the channel 23 by the DF1/EIP component. Target IP Address Route for channel 24: ;Target IP Address Route for the messages sent to the channel 24 by the DF1/EIP component. Target IP Address Route for channel 25: ;Target IP Address Route for the messages sent to the channel 25 by the DF1/EIP component. Target IP Address Route for channel 26: ;Target IP Address Route for the messages sent to the channel 26 by the DF1/EIP component. Target IP Address Route for channel 27: ;Target IP Address Route for the messages sent to the channel 27 by the DF1/EIP component. Target IP Address Route for channel 28: ;Target IP Address Route for the messages sent to the channel 28 by the DF1/EIP component. Target IP Address Route for channel 29: ;Target IP Address Route for the messages sent to the channel 29 by the DF1/EIP component. Target IP Address Route for channel 30: ;Target IP Address Route for the messages sent to the channel 30 by the DF1/EIP component. Target IP Address Route for channel 31: ;Target IP Address Route for the messages sent to the channel 31 by the DF1/EIP component. Target IP Address Route for channel 32: ;Target IP Address Route for the messages sent to the channel 32 by the DF1/EIP component. Target IP Address Route for channel 33: ;Target IP Address Route for the messages sent to the channel 33 by the DF1/EIP component. Target IP Address Route for channel 34: ;Target IP Address Route for the messages sent to the channel 34 by the DF1/EIP component. Target IP Address Route for channel 35: ;Target IP Address Route for the messages sent to the channel 35 by the DF1/EIP component. Target IP Address Route for channel 36: ;Target IP Address Route for the messages sent to the channel 36 by the DF1/EIP component. Target IP Address Route for channel 37: ;Target IP Address Route for the messages sent to the channel 37 by the DF1/EIP component. Target IP Address Route for channel 38: ;Target IP Address Route for the messages sent to the channel 38 by the DF1/EIP component. Target IP Address Route for channel 39: ;Target IP Address Route for the messages sent to the channel 39 by the DF1/EIP component. Target IP Address Route for channel 40: ;Target IP Address Route for the messages sent to the channel 40 by the DF1/EIP component. Target IP Address Route for channel 41: ;Target IP Address Route for the messages sent to the channel 41 by the DF1/EIP component. Target IP Address Route for channel 42: ;Target IP Address Route for the messages sent to the channel 42 by the DF1/EIP component. Target IP Address Route for channel 43: ;Target IP Address Route for the messages sent to the channel 43 by the DF1/EIP component. Target IP Address Route for channel 44: ;Target IP Address Route for the messages sent to the channel 44 by the DF1/EIP component. Target IP Address Route for channel 45: ;Target IP Address Route for the messages sent to the channel 45 by the DF1/EIP component. Target IP Address Route for channel 46: ;Target IP Address Route for the messages sent to the channel 46 by the DF1/EIP component. Target IP Address Route for channel 47: ;Target IP Address Route for the messages sent to the channel 47 by the DF1/EIP component. Target IP Address Route for channel 48: ;Target IP Address Route for the messages sent to the channel 48 by the DF1/EIP component. Target IP Address Route for channel 49: ;Target IP Address Route for the messages sent to the channel 49 by the DF1/EIP component. Target E-Mail Address for channel 50: ;Target E-Mail Address for the messages sent to the channel 50 by the DF1/EIP component. Target E-Mail Address for channel 51: ;Target E-Mail Address for the messages sent to the channel 51 by the DF1/EIP component. Target E-Mail Address for channel 52: ;Target E-Mail Address for the messages sent to the channel 52 by the DF1/EIP component. Target E-Mail Address for channel 53: ;Target E-Mail Address for the messages sent to the channel 53 by the DF1/EIP component. Target E-Mail Address for channel 54: ;Target E-Mail Address for the messages sent to the channel 54 by the DF1/EIP component. Target E-Mail Address for channel 55: ;Target E-Mail Address for the messages sent to the channel 55 by the DF1/EIP component. Target E-Mail Address for channel 56: ;Target E-Mail Address for the messages sent to the channel 56 by the DF1/EIP component. Target E-Mail Address for channel 57: ;Target E-Mail Address for the messages sent to the channel 57 by the DF1/EIP component. Target E-Mail Address for channel 58: ;Target E-Mail Address for the messages sent to the channel 58 by the DF1/EIP component. Target E-Mail Address for channel 59: ;Target E-Mail Address for the messages sent to the channel 59 by the DF1/EIP component. Target E-Mail Address for channel 60: ;Target E-Mail Address for the messages sent to the channel 60 by the DF1/EIP component. Target E-Mail Address for channel 61: ;Target E-Mail Address for the messages sent to the channel 61 by the DF1/EIP component. Target E-Mail Address for channel 62: ;Target E-Mail Address for the messages sent to the channel 62 by the DF1/EIP component. Target E-Mail Address for channel 63: ;Target E-Mail Address for the messages sent to the channel 63 by the DF1/EIP component. Target E-Mail Address for channel 64: ;Target E-Mail Address for the messages sent to the channel 64 by the DF1/EIP component. Target E-Mail Address for channel 65: ;Target E-Mail Address for the messages sent to the channel 65 by the DF1/EIP component. Target E-Mail Address for channel 66: ;Target E-Mail Address for the messages sent to the channel 66 by the DF1/EIP component. Target E-Mail Address for channel 67: ;Target E-Mail Address for the messages sent to the channel 67 by the DF1/EIP component. Target E-Mail Address for channel 68: ;Target E-Mail Address for the messages sent to the channel 68 by the DF1/EIP component. Target E-Mail Address for channel 69: ;Target E-Mail Address for the messages sent to the channel 69 by the DF1/EIP component. Target E-Mail Address for channel 70: ;Target E-Mail Address for the messages sent to the channel 70 by the DF1/EIP component. Target E-Mail Address for channel 71: ;Target E-Mail Address for the messages sent to the channel 71 by the DF1/EIP component. Target E-Mail Address for channel 72: ;Target E-Mail Address for the messages sent to the channel 72 by the DF1/EIP component. Target E-Mail Address for channel 73: ;Target E-Mail Address for the messages sent to the channel 73 by the DF1/EIP component. Target E-Mail Address for channel 74: ;Target E-Mail Address for the messages sent to the channel 74 by the DF1/EIP component. Target E-Mail Address for channel 75: ;Target E-Mail Address for the messages sent to the channel 75 by the DF1/EIP component. Target E-Mail Address for channel 76: ;Target E-Mail Address for the messages sent to the channel 76 by the DF1/EIP component. Target E-Mail Address for channel 77: ;Target E-Mail Address for the messages sent to the channel 77 by the DF1/EIP component. Target E-Mail Address for channel 78: ;Target E-Mail Address for the messages sent to the channel 78 by the DF1/EIP component. Target E-Mail Address for channel 79: ;Target E-Mail Address for the messages sent to the channel 79 by the DF1/EIP component. Target E-Mail Address for channel 80: ;Target E-Mail Address for the messages sent to the channel 80 by the DF1/EIP component. Target E-Mail Address for channel 81: ;Target E-Mail Address for the messages sent to the channel 81 by the DF1/EIP component. Target E-Mail Address for channel 82: ;Target E-Mail Address for the messages sent to the channel 82 by the DF1/EIP component. Target E-Mail Address for channel 83: ;Target E-Mail Address for the messages sent to the channel 83 by the DF1/EIP component. Target E-Mail Address for channel 84: ;Target E-Mail Address for the messages sent to the channel 84 by the DF1/EIP component. Target E-Mail Address for channel 85: ;Target E-Mail Address for the messages sent to the channel 85 by the DF1/EIP component. Target E-Mail Address for channel 86: ;Target E-Mail Address for the messages sent to the channel 86 by the DF1/EIP component. Target E-Mail Address for channel 87: ;Target E-Mail Address for the messages sent to the channel 87 by the DF1/EIP component. Target E-Mail Address for channel 88: ;Target E-Mail Address for the messages sent to the channel 88 by the DF1/EIP component. Target E-Mail Address for channel 89: ;Target E-Mail Address for the messages sent to the channel 89 by the DF1/EIP component. Target E-Mail Address for channel 90: ;Target E-Mail Address for the messages sent to the channel 90 by the DF1/EIP component. Target E-Mail Address for channel 91: ;Target E-Mail Address for the messages sent to the channel 91 by the DF1/EIP component. Target E-Mail Address for channel 92: ;Target E-Mail Address for the messages sent to the channel 92 by the DF1/EIP component. Target E-Mail Address for channel 93: ;Target E-Mail Address for the messages sent to the channel 93 by the DF1/EIP component. Target E-Mail Address for channel 94: ;Target E-Mail Address for the messages sent to the channel 94 by the DF1/EIP component. Target E-Mail Address for channel 95: ;Target E-Mail Address for the messages sent to the channel 95 by the DF1/EIP component. Target E-Mail Address for channel 96: ;Target E-Mail Address for the messages sent to the channel 96 by the DF1/EIP component. Target E-Mail Address for channel 97: ;Target E-Mail Address for the messages sent to the channel 97 by the DF1/EIP component. Target E-Mail Address for channel 98: ;Target E-Mail Address for the messages sent to the channel 98 by the DF1/EIP component. Target E-Mail Address for channel 99: ;Target E-Mail Address for the messages sent to the channel 99 by the DF1/EIP component. E-Mail Server IP Address: 0.0.0.0 ;IP Address of the E-Mail Server all e-mail messages will be sent to E-Mail From String: ;The From: string that will be used when sending any e-mail message. Com1 DF1 Baud Rate: Auto ;Baud Rate used for the DF1 devices connected to the COM1 serial port Com2 DF1 Baud Rate: Auto ;Baud Rate used for the DF1 devices connected to the COM2 serial port Incoming IP Security Descriptor 1: 0.0.0.0 ;Security Descriptor 1 limits access for the incoming traffic to the specified range of IP addresses Incoming IP Security Descriptor 2: 0.0.0.0 ;Security Descriptor 2 limits access for the incoming traffic to the specified range of IP addresses MODBUS Listening Port: 502 ;MODBUS Transactions will be handled on this Port MODBUS Slave Format: MODBUS/RTU ;MODBUS RTU or ASCII serial mode MODBUS Slave Timeout: 500 ;MODBUS Slave Timeout ADR RSSI Delta: 5 ;RSSI delta used to calculate auto data rate ADR SNR Delta: 2 ;SNR delta used to calculate auto data rate ADR RSSI threshold: -87 ;RSSI threshold used to calculate auto data ADR SNR threshold: 26 ;SNR threshold used to calculate auto data rate Remote Mobility Enable: disabled ;Setting to enable optimizations for Mobility Database Logging: remotes ;Enable log levels for SDB User Auth Mode: PAP ;The RADIUS mode to be used to do user authentication Auth Server Address: 0.0.0.0 ;The IP Address of the RADIUS server for user authentication Auth Server Port: 1812 ;The IP Port of the RADIUS server for user authentication User Auth Method: Local ;The method of authentication to be used for users User Auth Fallback: None ;The fallback method of authentication to be used for users Device Auth Method: None ;The method of authentication to be used for this device SSH Access: enabled ;Setting to enable the SSH interface Web Mode: HTTP ;The mode to use for web access (HTTP/HTTPS) Rem-to-Rem Bridging: enabled ;Determines whether this AP's remotes can pass data to one another. Prioritized AP's: disabled ;Setting to allow a remote to scan for preferred AP's Priority AP 1: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 2: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 3: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 4: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 5: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 6: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 7: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 8: 00:00:00:00:00:00 ;Hardware address of a priority AP Priority AP 9: 00:00:00:00:00:00 ;Hardware address of a priority AP Certificate TFTP Host IP: 192.168.1.1 ;IP Address of the TFTP Host from which certificates are downloaded Certificate Filename: ca-cert ;File name on the TFTP Host of the certificate to download Certificate Type: Root Certificate ;The type of certificate to download Priority AP Scan Time: 10 ;Seconds for remote to wait for beacon from highest priority AP Priority AP Connection Time: 60 ;Minutes for remote to stay connected until rescanning Ethernet Port Status: Always On ;The status of ethernet port. ImmMcast Flag: enabled ;(RO) Determines whether this AP sets the immMcast flag in the TxControl Field. VLAN Status: disabled ;Enable/Disable use of seperate VLANs for Management and Data traffic VLAN Ethport Mode: auto ;VLAN Ethernet Port Mode - auto|trunk|access Management VLAN ID: 2 ;VLAN ID for Management packets Data1 VLAN ID: 3 ;VLAN ID for Data1 packets Default Route IF: mgmt ;Network Interface Port for default route Data1 VLAN IP Address: 192.168.2.1 ;The IPv4 Data1 VLAN address of this unit. This field unnecessary if DHCP enabled on Data VLAN. Data1 VLAN IP Netmask: 255.255.255.0 ;The IPv4 Data1 VLAN subnet mask. This field unnecessary if DHCP enabled on Data VLAN. Data1 VLAN IP Gateway: 0.0.0.0 ;The IPv4 Data1 VLAN address of the network gateway device, typically a router. This field unnecessary if DHCP enabled on Data VLAN. Blacklist Timer: 10 ;The number of seconds before aging out an AP fro mthe blacklist Settling Timer: 10 ;The number of seconds to wait before attempting to find a better AP Auth Server Port: 1812 ;The IP Port of the RADIUS server for user authentication Management VLAN Mode: tagged ;Management VLAN mode, tagged or untagged/native