; Default Configuration Script for MDS iNET 900, version 5.1.0 ; IP Address: 192.168.1.1 ;The IPv4 address of this unit. This field is unnecessary if DHCP is enabled. Caution!!! Changing this value via the network will cause a loss of communication. IP Netmask: 255.255.0.0 ;The IPv4 local subnet mask. This field is unnecessary if DHCP is enabled. IP Gateway: 0.0.0.0 ;The IPv4 address of the network gateway device, typically a router. This field is unnecessary if DHCP is enabled. Model Number: 900 ;(RO) The model number of this unit. This value is set by the factory and cannot be changed. DHCP Client: disabled ;Dynamic Host Configuration Protocol Client. When enabled, the IP address, netmask and gateway will be automatically configured. Note that a device running as a DHCP server must be present on the local network to fulfill the DHCP request and powerup. Unit Name: ;A name for this unit. It appears at the top of every menu screen. Owner: ;The name of the owner of this unit. Contact: ;The contact person regarding this unit. Description: ;A brief general description of this unit. Location: ;The location of this unit. Com1 Byte Format: 8N1 ;Configuration of character size, type of parity, and number of stop bits to be used. Com2 Byte Format: 8N1 ;Configuration of character size, type of parity, and number of stop bits to be used. Max Remotes Allowed: 50 ;The maximum number of remotes allowed to connect to this Access Point. Device Mode: Remote ;Configures the unit to act as a Remote or an Access Point . The Access Point option is not allowed unless the unit is specifically ordered as such, or an authorization key has been purchased to allow it. Dwell Time: 65.5 ;The amount of time the unit spends at any given frequency in its hopping pattern. This field is only changable by a Master. Remotes read the Masters value upon association. Hop Pattern: 1 ;A seed used to create the pseudo-random hopping pattern Lan Enable: enabled ;Enable or Disable the Ethernet LAN port. Network Name: Not Programmed ;The name of the network this unit belongs to. The unit will only communicate with devices having identical network names. Date Format: Generic ;Specifies the format of the date. Generic=dd Mmm yyyy. European=dd-mm-yyyy. US=mm-dd-yyyy. Console Baud: 19200 ;The baud rate of the serial menu console. Default value is 19200 bps. Company Name: MDS ;(RO) The name of the product manufacturer. Version Name: 06-6000A01 ;(RO) The software part number. Product Name: iNET ;(RO) The name of this device Beacon Period: Normal ;The amount of time in milliseconds between beacon transmissions by the AP Data Rate: 256kbps ;The selected over-the-air data rate. A lower data rate generally allows more distance between the unit and its Master. Association Events: disabled ;Enable/Disable Association Events RF Output Power Setpoint: 30 ;The desired amount of RF output power, measured in dBm. Skipped Hop Zone1: Active ;The configured RF zones to skip Skipped Hop Zone2: Active ;The configured RF zones to skip Skipped Hop Zone3: Active ;The configured RF zones to skip Skipped Hop Zone4: Active ;The configured RF zones to skip Skipped Hop Zone5: Active ;The configured RF zones to skip Skipped Hop Zone6: Active ;The configured RF zones to skip Skipped Hop Zone7: Active ;The configured RF zones to skip Skipped Hop Zone8: Active ;The configured RF zones to skip Skipped Hop Zone9: Active ;The configured RF zones to skip Skipped Hop Zone10: Active ;The configured RF zones to skip Firmware TFTP Host IP: 127.0.0.1 ;IP Address of the TFTP Host from which firmware images are downloaded Firmware TFTP Filename: ;File name on the TFTP Host of the firmware image to download Eventlog TFTP Host IP: 127.0.0.1 ;IP Address of TFTP Host to which to send the event log Eventlog TFTP Filename: ;File name on the TFTP Host of the event log Config Script TFTP Host IP: 127.0.0.1 ;TFTP Host to which configuration scripts will be sent and received. Config Script TFTP Filename: ;File name of the configuration script. Fragmentation Threshold: 1600 ;Max packet size allowed before fragmentation occurs RTS Threshold: 500 ;Number of bytes for the RTS/CTS handshake boundary RSSI Threshold: -90 ;RSSI value at which the connection is deemed 'degraded' SNR Threshold: 0 ;SNR value at which the connection is deemed 'degraded' SNMP Read Community: public ;Community string for read access using SNMPv1 SNMP Write Community: private ;Community string for write access using SNMPv1 SNMP Trap Community: public ;Community string sent with traps using SNMPv1 SNMP Trap Manager #1: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent SNMP Trap Manager #2: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent SNMP Trap Manager #3: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent SNMP Trap Manager #4: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent Auth trap enable: disabled ;Setting to enable SNMP authentication traps Trap Version: v1 Traps ;Selects which SNMP trap format to send TFTP Timeout: 10 ;Timeout, in seconds, for TFTP file transfers Remote Database Timeout: 5 ;Timeout, in minutes, for ageing Remotes and Endpoints out of the Remote Database Com1 Serial Data Enable: disabled ;Setting to enable COM1 data mode Com1 Serial Data Baud Rate: 9600 ;Baud rate for COM1 data mode Com1 Serial Data Remote IP Address: 0.0.0.0 ;COM1 data will be sent to this IP address Com1 Serial Data Remote IP Port: 30010 ;COM1 data will be sent to this IP port Com1 Serial Data Local IP Port: 30010 ;COM1 data will be received on this IP port Com2 Serial Data Enable: enabled ;Setting to enable COM2 data mode Com2 Serial Data Baud Rate: 9600 ;Baud rate for COM2 data mode Com2 Serial Data Remote IP Address: 0.0.0.0 ;COM2 data will be sent to this IP address Com2 Serial Data Remote IP Port: 30011 ;COM2 data will be sent to this IP port Com2 Serial Data Local IP Port: 30011 ;COM2 data will be received on this IP port Com2 Serial Data Flow Control: disabled ;Setting to enable hardware flow control (RTS/CTS) in COM2 data mode SNTP Server IP: 0.0.0.0 ;The IPv4 address of NTP/SNTP Time Server Com1 Serial Data Seamless Mode: disabled ;Setting to enable seamless mode for COM1 data mode Com2 Serial Data Seamless Mode: disabled ;Setting to enable seamless mode for COM2 data mode Com1 Serial Data Delimiter Chars: 4 ;Minimum number of characters which will be considered a gap in seamless mode for COM1 Com2 Serial Data Delimiter Chars: 4 ;Minimum number of characters which will be considered a gap in seamless mode for COM2 Com1 Serial Data Buffer Size: 64 ;Number of output characters which will be buffered in seamless mode for COM1 Com2 Serial Data Buffer Size: 64 ;Number of output characters which will be buffered in seamless mode for COM2 RF Frequency Hopping Format: USA/CANADA ;(RO) The frequency-hopping rules the radio is configured to operate under Hop Protocol: 1 ;Frequency hopping protocol version DHCPd Server Enable: disabled ;Enable/Disable DHCP Server Daemon DHCPd Netmask: 0.0.0.0 ;The IP Address to be used as the DHCP Netmask DHCPd Start Address: 0.0.0.0 ;The IP Address to be used as the starting address DHCPd End Address: 0.0.0.0 ;The IP Address to be used as the ending address DHCPd DNS Address: 0.0.0.0 ;The IP Address to be used as the DNS Address DHCPd WINS Address: 0.0.0.0 ;The IP Address to be used as the WINS Address Approved Remotes List Enable: disabled ;Setting to enable the Approved Remotes List Encryption Enable: disabled ;Setting to enable over-the-air data encryption HTTP Enable: enabled ;Setting to enable the HTTP interface Telnet Enable: enabled ;Setting to enable the Telnet interface HTTP MD5 Authentication: disabled ;Setting to enable MD5 Digest Authentication Automatic Key Rotation: enabled ;Setting to enable Automatic Key Rotation Approved APs List Enable: disabled ;Setting to enable the Approved Access Points List Watch-Link-Status Flag @ AP: disabled ;A flag that controls whether the Remotes care about the AP's Ethernet Link Status Syslog Server Address: 0.0.0.0 ;The IPv4 address of a syslog server Ethernet Rate Limit: 500000 ;Ethernet traffic rate limit on Ethernet Port. (used for monitoring) Com1 Serial Data Multicast IP Port: 30010 ;COM1 data will be sent/recieved to this IP port, depending on data mode Com2 Serial Data Multicast IP Port: 30011 ;COM2 data will be sent/recieved to this IP port, depending on data mode Com1 Serial Data Primary TCP Client IP Address: 0.0.0.0 ;COM1 data will be sent to this IP address Com1 Serial Data Primary TCP Client IP Port: 30010 ;COM1 data will be sent to this IP port Com1 Serial Data Secondary TCP Client IP Port: 30010 ;COM1 data will be sent to this IP port Com1 Serial Data Secondary TCP Client IP Address: 0.0.0.0 ;COM1 data will be sent to this IP address Com2 Serial Data Primary TCP Client IP Address: 0.0.0.0 ;COM2 data will be sent to this IP address Com2 Serial Data Primary TCP Client IP Port: 30011 ;COM2 data will be sent to this IP port Com2 Serial Data Secondary TCP Client IP Port: 30011 ;COM2 data will be sent to this IP port Com2 Serial Data Secondary TCP Client IP Address: 0.0.0.0 ;COM2 data will be sent to this IP address Com1 Serial Data TCP Outgoing Keepalive: 5 ;Com1 TCP connection will be reset after this period of inactivity Com2 Serial Data TCP Outgoing Keepalive: 5 ;Com2 TCP connection will be reset after this period of inactivity Com1 Serial Data TTL: 1 ;Com1 TCP Time-To-Live Value Com2 Serial Data TTL: 1 ;Com2 TCP Time-To-Live Value Com1 Serial Data PPP Address: 0.0.0.0 ;Com1 IP address for connected PPP device Com2 Serial Data PPP Address: 0.0.0.0 ;Com2 IP address for connected PPP device Com1 Serial Data Multi Packet Sends: 6 ;Com1 redundant UDP packet sends Com2 Serial Data Multi Packet Sends: 6 ;Com2 redundant UDP packet sends Snmp v3 password mode: MANAGER ;Snmp v3 password mode Snmp v3 auth password: MDSAuthPwd ;Snmp v3 auth password Snmp v3 priv password: MDSPrivPwd ;Snmp v3 priv password AP Automatic Remote Upgrade Feature: disabled ;AP Automatic Remote Upgrade Feature AP Reboot mode for Remotes: disabled ;Tells Remote whether to reboot or not after upgrade Poll Address: 0.0.0.0 ;The IP Address to be polled for link status Compress Enable: disabled ;Enable/Disable compression of frames over the air. Com1 UDP Packet Repeat Mode: disabled ;Com1 Turns on Packet Transmittion and Reception of Multiple UDP Packets Com2 UDP Packet Repeat Mode: disabled ;Com2 Turns on Packet Transmittion and Reception of Multiple UDP Packets Com1 Serial Data TCP Incoming Keepalive: 600 ;Com1 TCP connection will be reset after this period of inactivity Com2 Serial Data TCP Incoming Keepalive: 600 ;Com2 TCP connection will be reset after this period of inactivity Com1 Serial Data Multicast Address: 224.0.0.0 ;COM1 data will be sent/received on this IP address, depending on data mode Com2 Serial Data Multicast Address: 224.0.0.0 ;COM2 data will be sent/received on this IP address, depending on data mode Com1 Serial Data IP Mode: UDP_P2P ;IP Protocol for COM1 data mode Com2 Serial Data IP Mode: UDP_P2P ;IP Protocol for COM2 data mode UTC Time Offset: 0 ;Difference between yout time and UTC time.