; MDS entraNET AP 900 Standard Default Configuration Script ; Created Thurs Mar 1 2007 Location: ;The physical location of this device Device Name: ;An identification for this device Description: ;A description of this product Contact: ;Contact information for the administration of this device Date Format: Generic ;The format in which the date should be displayed Static IP Address: 192.168.1.1 ;The IP address of this device Static IP Netmask: 255.255.0.0 ;The IP netmask of this device Static IP Gateway: 0.0.0.0 ;The IP gateway of this device IP Address Mode: Static ;Use static IP addressing or dynamic IP addressing using DHCP TFTP Host Address: 127.0.0.1 ;The IP Address of the TFTP server for firmware Firmware Filename: firmware.gpk ;The filename of the firmware package on the TFTP server Syslog Server Address: 127.0.0.1 ;The IP Address of the Syslog server Config Filename: cfgscript.txt ;The filename of the configuration script on the TFTP server Console Baud Rate: 19200 ;The baud rate of the console port TFTP Timeout: 30 ;The TFTP timeout in seconds Max Remotes: 100 ;The maximum number of remotes that may connect to this master Encryption Enable: disabled ;Enable encryption of over-the-air data Database Timeout: 10 ;A maximum period of inactivity for a remote or endpoint FEC: disabled ;Enable Forward error correction on the radio network RF Output Power: 30 ;Configure the internal radio's transmitter power Dwell Time: 14 msec ;Configure the dwell time in milliseconds (14,28 or 7) Skip Zones: 0 ;Configure the frequency skip zones Net Address: 0 ;The address of the radio network Broadcast Repeat Count: 3 ;The number of times a broadcast frame is repeated Unicast Retry Count: 10 ;The number of times a unicast frame is retried X Address: 0 ;The radio's X Address for multi-Access Point networks Com 1 Mode: Unicast UDP ;Mode of operation for COM1 Com 1 TX IP Address: 0.0.0.0 ;Destination IP address for COM1 UDP data packets Com 1 TX IP Port: 1024 ;Destination IP port for COM1 UDP data packets Com 1 RX IP Port: 30010 ;IP port for UDP recieve Com 1 Port Status: disabled ;Enable/disable data mode on COM1 Com 1 Baud Rate: 19200 ;Baud rate for COM1 data mode Com 1 Byte Format: 8N1 ;Character size, parity, and stop bits for COM1 data mode Com 1 Remote UnitID: 1 ;Destination unit ID of remote unit for serial-to-serial mode Com 2 Port Status: disabled ;Enable/disable data mode on COM2 Com 2 Mode: Unicast UDP ;Mode of operation for COM2 Com 2 TX IP Address: 0.0.0.0 ;Destination IP address for COM2 UDP data packets Com 2 TX IP Port: 1024 ;Destination IP port for COM2 UDP data packets Com 2 RX IP Port: 30011 ;IP port for UDP recieve Com 2 Baud Rate: 19200 ;Baud rate for COM2 data mode Com 2 Byte Format: 8N1 ;Character size, parity, and stop bits for COM2 data mode Com 2 Remote UnitID: 1 ;Destination unit ID of remote unit for serial-to-serial mode Approve Remotes: disabled ;Enable Remote association filtering based on the Approved Remotes list Telnet Access: enabled ;Enable telnet access HTTP Acccess: enabled ;Enable access via the web interface Address to Ping: 127.0.0.1 ;IP Address of a host to ping Event Log Host Address: 0.0.0.0 ; Event Log Filename: eventlog.txt ; BSP Routing Enable: disabled ;Enable routing of BSP packets IAPP Enable: disabled ;Enable routing of BSP packets between APs Unit Update Enable: disabled ;Enable immediate updates of database changes over IAPP Com 1 Inter-Packet Delay: 4 ;The minimum time between rx packets Com 2 Inter-Packet Delay: 4 ;The minimum time between rx packets HTTP Security Mode: Basic Auth ;Set HTTP login security type to BasicAuth or MD5 Trap Manager #1: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent Trap Manager #2: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent Trap Manager #3: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent Trap Manager #4: 0.0.0.0 ;IP Address of a SNMP manager to which traps will be sent Auth Trap Enable: disabled ;Setting to enable SNMP authentication traps SNMP v3 Password Mode: manager ;SNMP v3 password mode Trap Version: v1 traps ;Selects which SNMP trap format to send SNMP Mode: v1-v2-v3 ;Set SNMP Agent Operating Mode RSG TalkBack Enable: disabled ;Enable RSG UDP connections to talk back to sender RSG TalkBack Timeout: 30 ;How long to keep the talk back address valid Com 1 Buffer Size: 64 Bytes ;The size of lowlevel buffer(s) Com 2 Buffer Size: 64 Bytes ;The size of lowlevel buffer(s) Com 1 Remote COM Port: Com 2 ;The remote serial port to be used Com 2 Remote COM Port: Com 2 ;The remote serial port to be used Com 1 Talkback Enable: disabled ;Enable COM1 UDP connections to talk back to sender Com 1 Talkback Timeout: 30 ;How long to keep the talk back address valid Com 2 Talkback Enable: disabled ;Enable COM2 UDP connections to talk back to sender Com 2 Talkback Timeout: 30 ;How long to keep the talk back address valid Ethernet Bridging: All ;Specify what types of ethernet frames to bridge Contention Window Min: 2 ;Minimum contention window value Contention Window Max: 10 ;Maximum contention window value Bridge Priority: 32769 ;Sets the bridge's relative priority Bridge Hello Time: 2 ;Time between transmission of Hello messages Bridge Forward Delay: 5 ;Time that the bridge waits before beginning forwarding IAPP Multicast Address: 224.254.1.1 ;Multicast IP address used by IAPP IAPP Multicast Port: 39990 ;Multicast IP port used by IAPP IAPP Multicast TTL: 1 ;Multicast packet time-to-live used by IAPP IAPP Unicast Port: 39991 ;Unicast IP port used by IAPP RSG Config Host Address: 0.0.0.0 ; RSG Config Filename: rsgcfg.txt ; Redundancy Configuration: disabled ;Enable Redundancy Network Interface Error: disabled ;Network Interface Error Frequency Not Calibrated: disabled ;Frequency Not Calibrated Power Not Calibrated: disabled ;Power Not Calibrated Lack of Remotes for: 500 ;Redundant Switchover if AP has no Assoc Remotes for spec time Maximum Receive Errors: 300 ;Redundant Switchover if # recv errors reaches ____ Receive Error Count Interval: 300 ;Redundant Switchover if # recv errors reached in ___time Hop Band: Band A ;Selectable Band for 2.4GHz Operation EndPoint Logging: enabled ;Turn on or off the event log entries for adding EndPoints DNP Routing Enable: disabled ;Enable routing of DNP packets DNP Multicast Address: 224.254.1.1 ;Multicast IP address used by DNP DNP Multicast Port: 20000 ;Multicast IP port used by DNP DNP Unicast Port: 20001 ;Unicast IP port used by DNP Com 1 TCP Keepalive: 5 ;Com 1 TCP connection will be reset after this period of inactivity Com 2 TCP Keepalive: 5 ;Com 2 TCP connection will be reset after this period of inactivity Package to Transmit: 1 ;Image to reprogram remotes Remote Access Mgr: disabled ;Enable management of approved remotes via 3rd-tier application Remote Access IP: 239.254.1.10 ;Multicast address to use when running Remote Access Manager