Software/Firmware Downloads
This directory contains the files necessary to upgrade LEDR software
to function with multiple E1 operation.
***************************************************************************
!!! NOTE !!!
The files in this directory are intended as a patch onto the LEDR code
base. They include only the necessary files to make a LEDR radio E1
capable. For all other files please download the original LEDR code
into the radio before applying this patch.
***************************************************************************
The file "LEDR_full_rate_version 103.zip" contains the following files:
E1_103.mpk - The binary image which is to be loaded into the
LEDR radio using the serial FlashUtil program or over a
network connection using TFTP. Please see the release notes
for the full LEDR software package for additional information
concerning the software upgrade process.
Release Notes for Full Rate E1 LEDR Update.doc - The release
notes detailing new features and modifications to the
software.
|